Viewing and changing values in the Basic menu - PENN Controls - A421ABD - A421AED - Electronic Temperature Control - A421 Off‐Cycle Defrost Model

A421 Series Electronic Temperature Controls with Off-Cycle Defrost Installation Guide

Brand
PENN Controls
Product name
A421 Off‐Cycle Defrost Model
Document type
Installation Guide
Part number
24-7664-3035
Document revision
E
Revision date
2022-08-25
Language
English

About this task

In this task you access the Basic menu and view and change the Basic parameter values.

Procedure

  1. On the Main screen, press MENU. The LCD displays OFF, which is the first parameter code screen displayed in the Basic menu.
  2. To scroll through all of the basic parameter codes and display the preferred code, press Down or Up
  3. With the preferred parameter code displayed, press MENU to display the current parameter value for the code.
  4. With the current parameter value displayed, press Down or Up to scroll through all of the parameter’s usable values and display the preferred value.
  5. With the preferred parameter value displayed, press MENU to save the displayed value and go to the next parameter code.
  6. To exit the Basic menu and go to the Advanced menu, simultaneously press and hold Down and Up, for 5 seconds.