Dimensions - PENN Controls - LIT-12012249 - A421AET - A421ABT - Electronic Temperature Control - A421 Series Electronic Temperature Control

A421 Series Electronic Temperature Controls with Cycle Timer Product Bulletin

Product
Controls > Electromechanical Temperature Controls > A421 Series Electronic Temperature Control
Document number
LIT-12012249
Revision date
2023-01-09

The following figure shows the dimensions of the A421 control with Type 1/IP20 enclosure.

Figure 1. A421ABT control, dimensions, in. (mm)