Adjustable sensor offset - PENN Controls - LIT-12012249 - A421ABT - A421AET - Electronic Temperature Control - A421 Duty‐Cycle/Ventilation Models

A421 Series Electronic Temperature Controls with Cycle Timer Product Bulletin

Brand
PENN Controls
Product name
A421 Duty‐Cycle/Ventilation Models
Document type
Product Bulletin
Document number
LIT-12012249
Revision date
2023-01-09
Language
English

Use the sensor temperature offset feature to offset the temperature displayed on the LCD from the temperature sensed at the A99 sensor. This feature is useful when the displayed temperature is different from the temperature measured at the sensor.