Features - PENN Controls - LIT-1927115 - A28AK - Electromechanical Temperature Control - A28 Series Two-Stage Temperature Control

A28AK Series Two-Stage Flange Mounted Duct Temperature Control Catalog Page

Product
Controls > Electromechanical Temperature Controls > A28 Series Two-Stage Temperature Control
Document type
Catalog Page
Document number
LIT-1927115
Revision date
07/03/2024
  • Flat flange mounting with a special coil element, to position the sensing bulb in the appropriate portion of the air stream
  • Two single-pole, double-throw (SPDT) snap-acting switches
  • Unaffected by barometric pressure or cross ambient temperatures