Description - PENN Controls - LIT-1927115 - A28AK - Electromechanical Temperature Control - A28 Series Two-Stage Temperature Control

A28AK Series Two-Stage Flange Mounted Duct Temperature Control Catalog Page

Product
Controls > Electromechanical Temperature Controls > A28 Series Two-Stage Temperature Control
Document number
LIT-1927115
Revision date
2024-03-07
Figure 1. A28AK temperature control

The A28AK is a two-stage temperature control with a special air coil sensing element and an adjustable mounting flange.

Refer to the A28 Series Two-Stage Temperature Controls with Type 1 Enclosure Product Bulletin (LIT-125130) for important product application information.