Wiring - PENN Controls - LIT-121055 - A19E - Electromechanical Temperature Control - A19 Duct Temperature Control

A19E Series Warm Air Fan and Duct Controls Low or Line Voltage Installation Guide

Product
Controls > Electromechanical Temperature Controls > A19 Duct Temperature Control
Document number
LIT-121055
Document revision
G
Revision date
2023-10-18
docpartnumberlabel
Part No.
Part number
997-653
CAUTION
  • Risk
  • Disconnect the power supply before wiring connections are made to avoid possible electrical shock or damage to equipment.

Follow the equipment manufacturer’s field diagrams if provided. Make all wiring to conform to the National Electrical Code and local regulations. Refer to the cover label of the control for the maximum electrical rating.

The wiring terminals of the single-pole, double-throw (SPDT) model are color coded for convenience and to simplify wiring. Red is the common terminal; red to yellow circuit closes on temperature increase, red to blue circuit opens on temperature increase. Use copper conductors only.

Important: Use the supplied 8-32 × 1/4 in. binder head terminal screws. Substitution of other screws could cause problems in making correct connections.