Fan control - PENN Controls - LIT-121055 - A19E - Electromechanical Temperature Control - A19 Duct Temperature Control

A19E Series Warm Air Fan and Duct Controls Low or Line Voltage Installation Guide

Product
Controls > Electromechanical Temperature Controls > A19 Duct Temperature Control
Document number
LIT-121055
Document revision
G
Revision date
2023-10-18
docpartnumberlabel
Part No.
Part number
997-653

The fan starts when the plenum temperature rises to the amount of the differential above the cutout setting. If the fan continues to run after furnace shutdown, increase the cutout setting. This also increases the fan cut-in setting.

Changing the differential changes the cut-in temperature only.