Duct temperature cutout control - PENN Controls - LIT-121055 - A19E - Electromechanical Temperature Control - A19 Duct Temperature Control

A19E Series Warm Air Fan and Duct Controls Low or Line Voltage Installation Guide

Product
Controls > Electromechanical Temperature Controls > A19 Duct Temperature Control
Document type
Installation Guide
Document number
LIT-121055
Document revision
G
Revision date
2023-10-18
docpartnumberlabel
Part No.
Part number
997-653

On a temperature rise to the cutout temperature, the control opens the circuit. The plenum cools down. When it cools by the amount of the differential, the contacts close.

You must manually reset the duct temperature cutout control after a lockout to close the circuit.