Mounting - PENN Controls - LIT-121055 - A19E - Electromechanical Temperature Control - A19 Duct Temperature Control

A19E Series Warm Air Fan and Duct Controls Low or Line Voltage Installation Guide

Product
Controls > Electromechanical Temperature Controls > A19 Duct Temperature Control
Document type
Installation Guide
Document number
LIT-121055
Document revision
G
Revision date
2023-10-18
docpartnumberlabel
Part No.
Part number
997-653

About this task

CAUTION
  • Risk
  • Do not dent or deform the sensitive bulb of this control. A dent or deformation changes the calibration and causes the control to cycle at a temperature lower than the dial setting.

Procedure

  1. Cut a 1 3/4 in. (35 mm) diameter hole in the plenum for the element.
  2. Use the flange as a template and mark the location for the two sheet metal mounting screws.
  3. Drill or punch mounting screw holes.
  4. Mount the flange to the plenum.
  5. Mount the control and tighten the lockscrew in the flange.