Installation - PENN Controls - LIT-121055 - A19E - Electromechanical Temperature Control - A19 Duct Temperature Control

A19E Series Warm Air Fan and Duct Controls Low or Line Voltage Installation Guide

Product
Controls > Electromechanical Temperature Controls > A19 Duct Temperature Control
Document number
LIT-121055
Document revision
G
Revision date
2023-10-18
docpartnumberlabel
Part No.
Part number
997-653

Follow the instructions supplied by the equipment manufacturer. Select a location in the plenum where the temperature element senses the average temperature and is in free air circulation. The element must not touch any internal part of the furnace.