Adjustments - PENN Controls - LIT-121055 - A19E - Electromechanical Temperature Control - A19 Duct Temperature Control

A19E Series Warm Air Fan and Duct Controls Low or Line Voltage Installation Guide

Product
Controls > Electromechanical Temperature Controls > A19 Duct Temperature Control
Document number
LIT-121055
Document revision
G
Revision date
2023-10-18
docpartnumberlabel
Part No.
Part number
997-653

There is an adjustment knob on the range screw. There is a dial pointer on the cutout stop bracket. The pointer on the duct controls indicates the temperature at which contacts open on temperature rise. On SPDT models the red to blue circuit opens on a temperature rise. On fan controls the dial pointer indicates the temperature at which the contacts open on a temperature drop.