Mounting the remote bulb - PENN Controls - A19CAC - Electromechanical Temperature Control - A19 Control for Hot Water Immersion

A19CAC Type Automatic Changeover Control Installation Guide

Product
Controls > Hot Water Controls > A19 Control for Hot Water Immersion
Document revision
J
Revision date
2023-10-18
docpartnumberlabel
Part No.
Part number
997-361

About this task

To mount the remote bulb, complete the following steps:

Figure 1. Remote bulb mount

Procedure

  1. Place the bulb against the pipe with the formed coils facing the pipe.
  2. Form the bulb to the contour of the pipe so that the bulb coils are against the pipe.
  3. Secure the bulb firmly against the pipe with high temperature electrical tape.
  4. Mount the control in any convenient location.