About this task
To mount the remote bulb, complete the following steps:
Figure 1. Remote bulb mount
Procedure
- Place the bulb against the pipe with the formed coils facing the pipe.
- Form the bulb to the contour of the pipe so that the bulb coils are against the pipe.
- Secure the bulb firmly against the pipe with high temperature electrical tape.
- Mount the control in any convenient location.