Mounting the control - PENN Controls - A19CAC - Electromechanical Temperature Control - A19 Control for Hot Water Immersion

A19CAC Type Automatic Changeover Control Installation Guide

Product
Controls > Hot Water Controls > A19 Control for Hot Water Immersion
Document revision
J
Revision date
2023-10-18
docpartnumberlabel
Part No.
Part number
997-361

About this task

To mount the control, complete the following steps:

Figure 1. Case, mounting plate, and mounting strap

Procedure

  1. Fasten the strap to the case with the clamp screw.
  2. Place the control on the tube or pipe and place the slot of the mounting strap over the tab on the case.
  3. Tighten the clamp screw to a snug fit.
    Important:
    • Do not tighten the clamp too tightly. Do not dent or crush the mounting plate, because it is also the temperature element. Any dent could result in a change of the control setting.
    • Do not place the strap inside the cover. Use the clamp screw to hold the strap to the control.
  4. Clip off or bend back the excess strapping.