Applications - PENN Controls - LIT-1927060 - A19CAC - Electromechanical Temperature Control - A19 Remote Bulb Control

A19CAC Series Automatic Changeover with Strap-On Mounting Catalog Page

Product
Controls > Bulb Controls > A19 Remote Bulb Control
Document type
Catalog Page
Document number
LIT-1927060
Revision date
2024-03-07

This control is designed for convectors, fan coils, blast coil units, and similar devices. The A19CAC-2 control can mount directly on either a vertical or a horizontal pipe, using the mounting strap supplied with the control. The A19CAC-1 control has a remote bulb for greater mounting convenience.

Figure 1. A19 Series switch action

Note: On a temperature increase above the set point, the circuit from red to blue (RB) opens, and simultaneously red to yellow (RY) closes.