Mounting - PENN Controls - A19BAC - A28AA - Electromechanical Temperature Control - A19 Coiled Bulb Control - A28 and A36 Multi‐Stage Temperature Control

A19BAC, A28AA Single and Two-Stage Space Thermostats for Heating and Ventilation Applications Installation Guide

Product
Controls > Electromechanical Pressure Controls > A19 Coiled Bulb Control
Document type
Installation Guide
Document revision
G
Revision date
2023-10-18
Part number
996-238
NOTICE
  • Risk of Property Damage.
  • Do not dent or deform the sensing bulb. Dents or deformations in the sensing bulb can change the calibration, may cause the control to operate at temperatures other than the set point, and may result in other property damage. When the bulb mounting clip is used to mount the bulb near the refrigerant tubing, ensure the sheet metal screw does not pierce the tubing.

Mount the control to a flat surface with screws through the holes provided in the back of the frame.

Important: On rough mounting surfaces, use the top two mounting holes only. When these controls are mounted on an uneven surface using screws in all four holes, the case can twist enough to affect the temperature control's calibration and operation.

Mount the control where it is exposed to the average temperature of the controlled space. Do not mount the control where it is affected by unusual heat or cold, such as directly over an animal stall, in sunlight, or on an outside wall. Avoid locations near a door, window, or hay chute.