Before applying power, make sure installation and plug connections are according to job specifications. After completing the necessary checks and adjustments, an operational checkout is required.
Adjust the control set point to put the system in operation and observe at least three complete operating cycles to be sure that all components are functioning correctly.
If the system fails to operate, recheck the wiring, settings, and components.