Adjusting the Thermostat Set Point - PENN Controls - A19AAT - Electromechanical Temperature Control - A19 Remote Bulb Control

A19AAT Type Cooling Thermostats for Portable Applications Installation Guide

Product
Controls > Bulb Controls > A19 Remote Bulb Control
Document revision
B
Revision date
2019-03-07
Part number
24-7664-2578

Adjust the set point using the external adjustment knob. The set point adjustment range on the A19AAT‐2C model thermostat is 20 to 80°F (-7 to 27°C).

The thermostat temperature differential is factory set at 3.5F° (2C°) and is not adjustable.