Mounting - PENN Controls - A19AAT - Electromechanical Temperature Control - A19 Remote Bulb Control

A19AAT Type Cooling Thermostats for Portable Applications Installation Guide

Product
Controls > Bulb Controls > A19 Remote Bulb Control
Document revision
B
Revision date
2019-03-07
Part number
24-7664-2578
WARNING
  • Risk of Electric Shock
  • Disconnect all electric power sources from the device before removing the device cover. Contact with internal components carrying hazardous voltage can cause electric shock and may result in severe personal injury or death.
Avertissement
  • Risque de décharge électrique
  • Déconnecter toutes les sources d'alimentation électrique de l'appareil avant de déposer le capot de l'appareil. Tout contact avec des composants internes conducteurs de tensions dangereuses risque d'entraîner une décharge électrique et de provoquer des blessures graves, voire mortelles.

Mount the thermostat in an accessible location where the control body, electrical cord, capillary tube and sensing element are not subject to damage.

Mount the thermostat to a flat, vertical surface through the mounting holes in back of the case or hang the thermostat from a sturdy support using the beaded‐chain assembly included with the thermostat.

Refer to the assembly instruction included with the beaded-chain hanger assembly.

Important: Mounting an A19AAT type thermostat on a rough or uneven surface may warp the control case and cause the thermostat to operate out of the intended temperature range. When mounting to rough or uneven surfaces, use only the top two mounting holes at the back of the thermostat. To avoid warping the thermostat case, do not over tighten the mounting screws.