WARNING
Avertissement
Mount the thermostat in an accessible location where the control body, electrical cord, capillary tube and sensing element are not subject to damage.
Mount the thermostat to a flat, vertical surface through the mounting holes in back of the case or hang the thermostat from a sturdy support using the beaded‐chain assembly included with the thermostat.
Refer to the assembly instruction included with the beaded-chain hanger assembly.
Important: Mounting an A19AAT type thermostat on a rough or uneven surface may warp the control case and cause the thermostat to operate out of the intended temperature range. When mounting to rough or uneven surfaces, use only the top two mounting holes at the back of the thermostat. To avoid warping the thermostat case, do not over tighten the mounting screws.