CAUTION
NOTICE
Make all wiring to conform to the National Electrical Code and local codes. Wire SPDT models as shown in Figure 2. Use copper conductor only.
Before you apply power, ensure that the installation and wiring connections are according to job specifications.
Important: Use the supplied 8-32 x 1/4 in.
binder head terminal screws. Substitution of other screws could cause problems with
making connections.