Packing nut - PENN Controls - LIT-125045 - A19 - Electromechanical Temperature Control - A19 Remote Bulb Control

A19 Series Temperature Control Without Enclosure Product Bulletin

Product
Controls > Bulb Controls > A19 Remote Bulb Control
Document number
LIT-125045
Revision date
2024-09-18

For closed tank applications where the temperature does not fall below -35°F (-37°C) or exceed 250°F (121°C), the FTG13A-600R packing nut assembly is available. The maximum liquid pressure limit is 150 psig (1,034 kPa).

Use the packing nut with a Style 1 bulb with support tube for direct immersion applications.

For applications where the temperature or liquid pressure exceeds these limits, specify the following when you order the control: a Style 4 element with an all-metal packing nut as an integral part of the control.

Figure 1. FTG13A-600R packing nut assembly