Features - PENN Controls - LIT-1927005 - A11E - A11D - A11A - A11B - Electromechanical Temperature Control - A11 Low Temperature Cutout Control

A11 Series Low Temperature Cutout Controls Catalog Page

Product
Controls > Temperature Controls > A11 Low Temperature Cutout Control
Document number
LIT-1927005
Revision date
2021-08-20
  • Precision repeat accuracy: the control always senses at the coldest point across the full length of the sensing element. The control remains unaffected by ambient temperature at the diaphragm cup and the 4 ft (1.2m) capillary. Install a 20 ft (6.1 m) or 40 ft (12.2 m) sensing element in the controlled area.
  • Trip-free manual reset provides the option to reset the lever. Press and release the lever before operation resumes.
  • Precision snap-acting contacts in a dust protected enclosure provides for the A11 Control to operate to the fullest potential.
  • Direct reading scale provides easy-to-adjust setpoint. You can make adjustments from the top or bottom of the control.