Description - PENN Controls - LIT-1927005 - A11E - A11D - A11A - A11B - Electromechanical Temperature Control - A11 Low Temperature Cutout Control

A11 Series Low Temperature Cutout Controls Catalog Page

Product
Controls > Temperature Controls > A11 Low Temperature Cutout Control
Document number
LIT-1927005
Revision date
2021-08-20

The A11 Series Low Temperature Cutout Controls are available with single-pole, single-throw (SPST) or single-pole, double-throw (SPDT) contact action. Applications include the sensing of low temperature conditions to avoid over cooling or icing of hydronic coils, cooling coils, and liquid-handing pipes. The controls are compact and sturdy, and have an adjustable temperature setpoint range with a fixed differential. You can access the range adjustment screw at the bottom of the control, or at the top of the control when you remove the cover. A factory-set low temperature stop is available when specified.

Refer to the A11 Series Low Temperature Cutout Controls Product Bulletin (LIT-125010) for additional product application information.

Figure 1. A11 Series Low Temperature Cutout Control