WARNING
Avertissement
Observe the following guidelines when wiring a field controller:
Important: Do not exceed the controller electrical ratings. Exceeding controller
electrical ratings can result in permanent damage to the controller and void any
warranty.
Important: Use copper conductors with a rating of at least 75°C (167°F). Make
all wiring in accordance with local, national, and regional regulations.
Important: Electrostatic discharge can damage controller components. Use proper
electrostatic discharge precautions during installation, setup, and servicing to avoid
damaging the controller.
For detailed information on configuring and wiring an MS/TP Bus, FC bus, and SA bus, refer to the MS/TP Communications Bus Technical Bulletin (LIT-12011034).