Setting the Device Addresses - PEAK - PK-OEM1810-0 - PK-OEM1820-0 - Smart equipment controller - PEAK OEM 18 24 Volt SMART Equipment Controller

PEAK OEM 18 24 Volt SMART Equipment Controller Installation Guide

Product
Controls > Smart Equipment Controls > PEAK OEM 18 24 Volt SMART Equipment Controller
Document type
Installation Guide
Document revision
C
Revision date
2021-03-26
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-934

Use the local display or MAP Gateway to set up device addresses. PEAK field controllers are master devices on MS/TP SA buses. Before operating field controllers on a bus, you must set a valid and unique device address for each controller on the bus through the local display or MAP gateway. Device addresses 4 through 127 are the valid addresses for these controllers.

Refer to the MS/TP Communications Bus Technical Bulletin (LIT-12011034) for more information on field controller device addresses and how to set them on MS/TP buses.

Table 1. SA Bus Device Address Description
Device Address Use on Description
0

(Switch 128 Off)

Reserved for FC Bus Supervisory Controller (not for use on field controllers).
1 to 3

(Switch 128 Off)

Reserved for peripheral devices (not for use on field controllers).
4 to 127

(Switch 128 Off)

Used for MS/TP master devices (field controllers) that are hard-wired to an SA bus or FC bus.
0 to 3

(Switch 128 On)

Reserved addresses for wired subordinate devices (not for use on field controllers).
4 to 127

(Switch 128 On)

Valid for MS/TP Master field controllers on wireless FC Buses only (future).