SA Bus Port - PEAK - PK-OEM1810-0 - PK-OEM1820-0 - Smart equipment controller - PEAK OEM 18 24 Volt SMART Equipment Controller

PEAK OEM 18 24 Volt SMART Equipment Controller Installation Guide

Product
Controls > Smart Equipment Controls > PEAK OEM 18 24 Volt SMART Equipment Controller
Document revision
C
Revision date
2021-03-26
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-934

The Sensor (SA Bus) port on the middle left side of the controller (Figure 1) is an RJ-12, 6-position modular jack that provides a connection for the Bluetooth® Commissioning Converter, the VAV Balancing Tool, specified network sensors, or other SA Bus devices with RJ-12 plugs.

The Sensor port is connected internally to the SA bus terminal block. See Table 1 for more information. The Sensor Port pin assignment is shown in Figure 2.