Modbus Terminal Block - PEAK - PK-OEM1810-0 - PK-OEM1820-0 - Smart equipment controller - PEAK OEM 18 24 Volt SMART Equipment Controller

PEAK OEM 18 24 Volt SMART Equipment Controller Installation Guide

Product
Controls > Smart Equipment Controls > PEAK OEM 18 24 Volt SMART Equipment Controller
Document revision
C
Revision date
2021-03-26
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-934

The Modbus terminal block is a green, removable, 3-terminal plug that fits into a board-mounted jack.

Wire the removable Modbus terminal block plugs on the controller, and wire the other field controllers in a daisy-chain configuration using 3-wire twisted, shielded cable as shown in Figure 1. See Table 1 for more information.

The Modbus port communicates as a master Modbus device and connects to the Modbus network, which may consist of one-to-many subordinate Modbus devices. Each Modbus subordinate device has a unique Modbus Register table and must be configured within the application of the PEAK controller. The configuration and application of Modbus is identified by the PEAK support team and programmed based on OEM applications.

Figure 1. Modbus Terminal Block