SA Bus Terminal Block - PEAK - PK-OEM1810-0 - PK-OEM1820-0 - Smart equipment controller - PEAK OEM 18 24 Volt SMART Equipment Controller

PEAK OEM 18 24 Volt SMART Equipment Controller Installation Guide

Product
Controls > Smart Equipment Controls > PEAK OEM 18 24 Volt SMART Equipment Controller
Document revision
C
Revision date
2021-03-26
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-934

The SA Bus terminal block is a brown, removable, 4-terminal plug that fits into a board-mounted jack.

Wire the removable SA Bus terminal block plugs on the lower port of the Dual Stacked Connector to the controller, and wire the other SA bus devices in a daisy-chain configuration using 4-wire twisted, shielded cable as shown in Figure 1. See Table 1 for more information.

Figure 1. SA Bus Terminal Block Wiring

Note: The SA BUS PWR terminal supplies 15 VDC. The SA BUS PWR terminal can be used to connect (daisy chain) the 15 VDC power leads on the SA BUS.
Figure 2. Pin Number Assignments for SA Bus Ports on PEAK SMART Equipment Controllers