Commissioning the Controllers - PEAK - PK-OEM1810-0 - PK-OEM1820-0 - Smart equipment controller - PEAK OEM 18 24 Volt SMART Equipment Controller

PEAK OEM 18 24 Volt SMART Equipment Controller Installation Guide

Product
Controls > Smart Equipment Controls > PEAK OEM 18 24 Volt SMART Equipment Controller
Document type
Installation Guide
Document revision
C
Revision date
2021-03-26
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-934

Commission the PEAK OEM 18 controller with CCT 10.3 with the OEM package. The programming is finalized by the OEM or the Johnson Controls Center of Excellence for application development. You cannot modify this application in the field; changes must be completed by the OEM. All configuration and parameter changes are completed through the local display or MAP Gateway.