The PEAK OEM 18 24 Volt SMART Equipment Controller is part of the SMART Equipment Controller family. The PEAK 18 Series controllers run pre-engineered applications and provide the inputs and outputs required to monitor and control a wide variety of HVAC equipment.
PEAK OEM 18 field controllers operate on an RS-485 BACnet® MS/TP Bus as BACnet Advanced Application Controllers (B-AACs) and integrate into Johnson Controls® and third-party BACnet systems.
PEAK OEM 18 controllers include an integral real-time clock, which enables the controllers to monitor and control schedules, calendars, trends, and operate for extended periods of time as stand-alone controllers when offline from the system network.
Important: Use this PEAK OEM 18 24 Volt Controller only as an operating control.
Where failure or malfunction of the PEAK OEM controller could lead to personal injury or
property damage to the controlled equipment or other property, additional precautions
must be designed into the control system. Incorporate and maintain other devices, such
as supervisory or alarm systems or safety or limit controls, intended to warn of or
protect against failure or malfunction of the PEAK OEM controller.
Important : Utiliser ce PEAK OEM 18 24 Volt Controller
uniquement en tant que dispositif de contrôle de fonctionnement. Lorsqu'une défaillance
ou un dysfonctionnement du controller risque de provoquer des blessures ou d'endommager
l'équipement contrôlé ou un autre équipement, la conception du système de contrôle doit
intégrer des dispositifs de protection supplémentaires. Veiller dans ce cas à intégrer
de façon permanente d'autres dispositifs, tels que des systèmes de supervision ou
d'alarme, ou des dispositifs de sécurité ou de limitation, ayant une fonction
d'avertissement ou de protection en cas de défaillance ou de dysfonctionnement du PEAK
OEM controller.