Wireless network applications - PEAK - PK-IOM5731-0 - PK-IOM5711-0 - Input/output controller - PEAK IOM57 Input/Output Module

PEAK IOM57 Input/Output Modules Installation Guide

Product
Controls > Input/Output Controls > PEAK IOM57 Input/Output Module
Document revision
D
Revision date
2021-05-04
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-985

About this task

You can install the controller in a wireless application when you use a ZFR1811 Wireless Field Bus Router.

To configure a controller for use with the ZFR1811 Series Wireless Field Bus system:

Note: IOMs can talk wirelessly on an FC bus only.

Procedure

  1. On the front of the controller, connect the ZFR1811 Wireless Field Bus Router to the FC bus port (RJ-12 modular jack).
  2. Ensure that the controller’s device address DIP switches are set to the correct device address. See Setting the device addresses.
  3. Set DIP switch 128 to ON enables wireless operation on the controller.

    For more information about installing a controller in a wireless configuration, refer to the ZFR1811 Wireless Field Bus Router Installation Instructions (Part No. 24-10325-1).