SA/FC bus port - PEAK - PK-IOM5731-0 - PK-IOM5711-0 - Input/output controller - PEAK IOM57 Input/Output Module

PEAK IOM57 Input/Output Modules Installation Guide

Product
Controls > Input/Output Controls > PEAK IOM57 Input/Output Module
Document type
Installation Guide
Document revision
D
Revision date
04/05/2021
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-985

The SA/FC bus port on the front of the controller is an RJ-12, 6-position modular jack that provides a connection for devices on the SA bus, a Wireless Commissioning Converter, ZigBee® wireless dongle, or a ZFR1811 Wireless Router, depending on which bus the IOM is operating on.

The SA/FC bus port connects internally to the SA/FC bus terminal block. See Table 1 for more information. The SA/FC bus port pin assignment is also shown in Figure 1.

Figure 1. Pin number assignments for sensor, SA bus, and FC bus ports on controllers