About this task
Important: Electrostatic discharge can damage controller components. Use
proper electrostatic discharge precautions during installation, setup, and servicing
to avoid damaging the controller.
Important: Disconnect all power sources to the controller before you remove
the cover and change the position of any jumper or the EOL switch on the controller.
Failure to disconnect power before changing a jumper or EOL switch position can
result in damage to the controller and void any warranties.
The controller cover is held in place with four plastic latches that extend from the base and snap into slots on the inside of the housing cover.
To remove the controller cover, complete the following steps:
Procedure
- Place your fingernails under the two cover lift tabs on the sides of the housing cover and gently pry the top of the cover away from the base to release the cover from the two upper latches. See Figure 1 for information about the controller.
- Pivot the top of the cover further to release it from the lower two latches.
- Replace the cover by placing it squarely over the base, and then gently and evenly push the cover on to the latches until they snap into the latched position.