Maximum cable length versus load current - PEAK - PK-IOM5731-0 - PK-IOM5711-0 - Input/output controller - PEAK IOM57 Input/Output Module

PEAK IOM57 Input/Output Modules Installation Guide

Product
Controls > Input/Output Controls > PEAK IOM57 Input/Output Module
Document revision
D
Revision date
2021-05-04
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-985

Use Figure 1 to estimate the maximum cable length relative to the wire size and the load current in mA when you wire the inputs and outputs.

Note: Figure 1 applies to the low-voltage (<30 V) inputs and outputs only. The load that is connected to the relay and local electrical codes determines the required size and length for high-voltage (>30 V) relay outputs.
Figure 1. Maximum wire length for low-voltage (<30 V) inputs and outputs by current and wire size