Installation - PEAK - PK-IOM5731-0 - PK-IOM5711-0 - Input/output controller - PEAK IOM57 Input/Output Module

PEAK IOM57 Input/Output Modules Installation Guide

Product
Controls > Input/Output Controls > PEAK IOM57 Input/Output Module
Document type
Installation Guide
Document revision
D
Revision date
04/05/2021
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-985

Observe the following guidelines when you install a field controller:

  • Transport the controller in the original container to minimize vibration and shock damage.
  • Verify that all parts shipped with the controller.
  • Do not drop the controller or subject it to physical shock.