Commissioning the controllers - PEAK - PK-IOM5731-0 - PK-IOM5711-0 - Input/output controller - PEAK IOM57 Input/Output Module

PEAK IOM57 Input/Output Modules Installation Guide

Product
Controls > Input/Output Controls > PEAK IOM57 Input/Output Module
Document revision
D
Revision date
2021-05-04
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-985

Commission controllers with the Controller Configuration Tool (CCT) software, either using a Wireless Commissioning Converter, a ZigBee wireless dongle, or a BACnet router mode when connected to an NAE or NCE. Refer to the Controller Tool Help (LIT-12011147) for detailed information on commissioning controllers.