The PEAK IOM57 Field Controllers belong to the PEAK Controller family. Input/Output Module (IOM) controllers expand the number of points that are connected to an OEM SMART Equipment controller (PEAK) to monitor and control a wide variety of HVAC/R equipment.
PEAK IOM57 field controllers operate on an RS-485 BACnet® MS/TP bus as BACnet Application Specific Controllers (B-ASCs) and integrate into Johnson Controls® and third-party BACnet systems.