Intégration BACnet/SC - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Guide de configuration du système Metasys

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2024-01-24
Product status
Active

BACnet Secure Connect (BACnet/SC) is a recent update to the BACnet interoperability standard aimed at improving cybersecurity and network infrastructure integrity. BACnet/SC is defined in Annex AB of the ASHRAE 135-2020 BACnet protocol standard. BACnet/SC identifies a secure, encrypted datalink layer specifically designed to meet the requirements, policies, and constraints of IP networking infrastructures.

Depuis la version 12.0, BACnet/SC est pris en charge par les composants suivants, quand ces composants sont mis à niveau sur le terrain ou envoyés depuis l’usine avec le logiciel Version 12.0 :
  • Application and Data Server (ADS), ADS-Lite, Extended Application and Data Server (ADX), and Open Application Server (OAS) series application server software
  • NAE85 and LCS85 series software-based network engines
    Remarque : You need to purchase the M4-BACNETSC-0 add-on license to use BACnet/SC on the ADS, ADS-Lite, ADX, OAS, NAE85, or LCS85.
  • NAE55xx-3x, SNE, and SNC series network engines
  • VMA1930, FAC4911, CGE, and CVE series IP-based equipment controllers
    Remarque : You can upgrade existing VMA1930 units in the field to support BACnet/SC, but this model is discontinued from manufacturing.
The primary benefits of Metasys BACnet/SC compliance include the following:
  • Ensures Metasys follows the latest IT security and infrastructure protocols while still maintaining interoperability.
  • Addresses many concerns that IT departments have expressed over the original BACnet/IP protocol.

Pour plus de détails sur BACnet/SC, reportez-vous au document BACnet/SC Workflow Technical Bulletin (LIT-12013959) .