Introducción - Metasys - LIT-12013222 - M4-OASSTD-0 - M4-OASSCHRPT-0 - M4-OASSTD-SC3 - M4-OASSTD-SCS - M4-OASHIST-0 - M4-OASPPA-0 - M4-OASMIN-0 - M4-OASSTD-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASMIN-6 - Server - Open Application Server - 12.0

Guía de instalación del Servidor Abierto de Aplicaciones (OAS)

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Installation Guide
Document number
LIT-12013222
Version
12.0
Revision date
2023-02-07
Product status
Active

La configuración del servidor Metasys es una utilidad completa que instala el software OAS, los componentes de terceros requeridos por OAS y muchos de los componentes de Microsoft requeridos por el sistema Metasys. Las siguientes tablas muestran los componentes instalados por el instalador de Metasys Server, salvo que ya estén presente. Para el software que aparece en la columna Componentes y productos NO instalados, utilice los correspondientes programas de instalación para agregar esos componentes y aplicaciones, si procede.

Tabla 1. Components installed and not installed by the Metasys Server

Windows® components installed

Metasys products installed

Components and products not installed

  • Microsoft Internet Information Services (IIS)
  • Microsoft .NET Framework 4.7.2
  • Microsoft Visual C++ Runtime Libraries
  • Microsoft Message Queuing (MSMQ)
  • Microsoft SQL Server® 2017 Express CU17 64-bit (ADS only)
  • Microsoft .NET Framework 3.5.1
  • Server at Release 12.0
  • Metasys UI Release 6.0
  • Monitoring and Commanding API
  • Launcher 2.0
  • Metasys Advanced Reporting System (ADX only)
  • Software Manager Release 3.0
  • Metasys system databases
  • SQL Server software (full version)
  • SQL Server Management Studio Express
  • System Configuration Tool (SCT)
  • Metasys for Validated Environments (MVE) for ADX
  • Metasys Export Utility for ADS and ADX
  • Metasys Database Manager
  • Site Management Portal (SMP)
  • Johnson Controls System Configuration Tool (JCT)
Nota: The Metasys Server setup attempts to install Microsoft .NET Framework 3.5.1 component. If the computer on which you are installing the Metasys Server software does not have access to Windows Updates, the installation of this component fails. In this case, install .NET Framework 3.5.1 manually.
The following table lists the third-party components installed with the Metasys Server Setup at Release 12.0.
Tabla 2. Third-party components installed with the Metasys Server setup
Third-party component Brief description
Erlang OTP 23.2 (11.1.4) A required component for RabbitMQ functionality.
RabbitMQ Server 3.8.16 RabbitMQ is a service bus used to send notification messages to other services and is used for inter-process communication (messages) on the server.
Set Rate Limits IIS module that applies rate limiting to Metasys API calls. This module and settings do not apply to SMP or Metasys UI.
GraphDB GraphDB stores a portion of the Metasys site's configuration data to improve data querying.
Antes de ejecutar el instalador, asegúrese de completar los siguientes pasos:
  1. Compruebe que el equipo con OAS tiene un sistema operativo Windows compatible. Consulte Especificaciones técnicas del OAS.
  2. Verifique y cambie si es necesario el nombre del equipo para que coincida con los siguientes requisitos de denominación de Metasys:
    • que comience con una letra, no con un número.
    • que contenga un máximo de 15 caracteres.
    • que contenga solo letras de la A a la Z (en mayúscula o minúscula), números del 0 al 9, y guiones.
    • que no termine en las letras OAS.
    • que no contenga marcas diacríticas ni acentos.
      Nota: no utilice guiones bajos en el sistema Metasys.
  3. Configure el cortafuegos de Windows para garantizar que estén abiertos los puertos que el software de Metasys requiera. Consulte Configuración del firewall de Windows.
  4. Si instala OAS en un equipo que no sea de habla inglesa, deberá establecer la configuración regional del equipo y el idioma predeterminado utilizado por la base de datos de SQL Server en la misma configuración regional que el idioma predeterminado del sitio. Consulte Instalación del servidor Metasys en un idioma distinto del inglés.
  5. Si el equipo tiene varias tarjetas de red, configure la tarjeta de red que el software del servidor Metasys vaya a usar. Consulte Configuración de tarjetas de red adicionales.
  6. Asegúrese de que el equipo host del OAS tenga acceso a las actualizaciones de Windows. Si no lo hace, la instalación automática de Microsoft .NET Framework falla y hay que instalarlo manualmente.
  7. Si desea que el OAS utilice certificados de confianza en lugar de certificados autofirmados, configure los certificados en el servidor Metasys antes de instalar el software. De lo contrario, vaya al paso siguiente. Consulte Appendix: Certificate management and security.