Related documentation - Metasys - Part No. 24-10325-10 - MS-ZFR1811-0 - MS-ZFR1811-1 - MS-ZFRCBL-0 - MS-ZFRRPT-0 - MS-ZFRZCT-0 - Bulb controller - ZFR1811 Wireless Field Bus Router - 5

ZFR1811 Wireless Field Bus Router Installation Instructions

Product
Network and Communications > Wireless Devices > ZFR1811 Wireless Field Bus Router
Document type
Installation Guide
Document number
Part No. 24-10325-10
Document revision
L
Version
5
Revision date
01/02/2017

For further information on how to set up a field controller to work with the ZFR1811 Router, refer to the following documents:

  • FEC16 Field Equipment Controller Installation Instructions (Part No. 24-10143-136)
  • FEC26 Field Equipment Controller Installation Instructions (Part No. 24-10143-144)
  • IOM17 and IOM27 Input/Output Modules Installation Instructions (Part No. 24-1044-76)
  • IOM37 Input/Output Module Installation Instructions (Part No. 24-1044-84)
  • IOM47 Input/Output Module Installation Instructions (Part No. 24-1044-92)
  • VMA16 Series Variable Air Volume Controllers Installation Instructions (Part No. 24-10143-20)

Some connections require the use of the ZFRCBL wire harness. To use the ZFRCBL wire harness, make the connections as shown in Figure 4 and Figure 5. For more information on using the ZFRCBL accessory, refer to the Wireless Commissioning Converter Installation Instructions (Part No. 24-10108-2).