United States - Metasys - Part No. 24-10325-10 - MS-ZFR1811-0 - MS-ZFR1811-1 - MS-ZFRCBL-0 - MS-ZFRRPT-0 - MS-ZFRZCT-0 - Bulb controller - ZFR1811 Wireless Field Bus Router - 5

ZFR1811 Wireless Field Bus Router Installation Instructions

Product
Network and Communications > Wireless Devices > ZFR1811 Wireless Field Bus Router
Document type
Installation Guide
Document number
Part No. 24-10325-10
Document revision
L
Version
5
Revision date
01/02/2017

Compliance Statement (Part 15.19)

This device complies with Part 15 of the FCC Rules. Operation is subject to the following two conditions:

  1. This device may not cause harmful interference, and
  2. This device must accept any interference received, including interference that may cause undesired operation.

Warning (Part 15.21)

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.