Mounting - Metasys - Part No. 24-10325-10 - MS-ZFRCBL-0 - MS-ZFR1811-1 - MS-ZFR1811-0 - MS-ZFRRPT-0 - MS-ZFRZCT-0 - Bulb controller - ZFR1811 Wireless Field Bus Router - 5

ZFR1811 Wireless Field Bus Router Installation Instructions

Product
Network and Communications > Wireless Devices > ZFR1811 Wireless Field Bus Router
Document number
Part No. 24-10325-10
Document revision
L
Version
5
Revision date
01/02/2017
Part number
24-10325-10

When mounting the ZFR1811 Router to an enclosure, mount it to the top, bottom, or side of the enclosure. Do not mount the ZFR1811 Router in a horizontal orientation. See Figure 1.

Figure 1. Proper (Top) and improper (Bottom) mounting orientations