LED status - Metasys - Part No. 24-10325-10 - MS-ZFRCBL-0 - MS-ZFR1811-1 - MS-ZFR1811-0 - MS-ZFRRPT-0 - MS-ZFRZCT-0 - Bulb controller - ZFR1811 Wireless Field Bus Router - 5

ZFR1811 Wireless Field Bus Router Installation Instructions

Product
Network and Communications > Wireless Devices > ZFR1811 Wireless Field Bus Router
Document number
Part No. 24-10325-10
Document revision
L
Version
5
Revision date
01/02/2017
Part number
24-10325-10
Table 1. ZFR1811 router status LED

Name

Visual Indication of:

Descriptions

General Operation

Normal

operation

OFF Steady = No power (or normal operation for more than 2 hours).

OFF Steady with 1 Flash every 10 seconds = ZFR1811 Router is not a member of a wireless network, invalid PAN OFFSET setting, no ZFR1810 Coordinators or ZFR1811 Routers in area.

ON Steady with Signal Strength displayed once every 10 seconds = ZFR1811 Router is a member of a wireless network.

OFF Steady with Signal Strength displayed once every 10 seconds = Wireless network is actively communicating, but ZFR1810 Coordinator cannot be reached (for example, coordinator lost power).

Signal Strength Indication 1

Wireless signal

strength

3 Flashes - Excellent

2 Flashes - Good

1 Flash - Weak

OFF for 3 seconds - None

Network Reform

Operation

during network

reform

Rapid Flashes for 5 minutes = rapid flashes occur for up to 5 minutes:

  • when the Reform Network option is initiated to the network, the ZFR1811 Router disconnects itself from the network
  • when the PAN OFFSET is changed on the ZFR1811 Router
  • when the PAN OFFSET is changed on the ZFR1811 Router after it has already joined another PAN
  • when the Channel Mask in the ZFR1810 is changed from CCT

Network Ping

Wireless node

function in the

network

Network pings provide a means of physically locating connected devices. There are two

methods with different use cases:

1) Use ZFR Checkout Tool (ZCT) to ping an address. This LED on the connected ZFR1811

to blink, indicating the device mapped to that specific MS/TP address

2) Press the Occupancy pushbutton on a WRZ Network Sensor. This causes the blinking

response on the ZFR1811 connected to the paired device. This can be used to validate

switch settings on the sensor during installation.

1 The Signal Strength LEDs on all the ZFR1811 Routers in a network extinguish after approximately 2 hours or normal operation, making the ZFR1811 less distracting when installed in an open area. To re-enable the ZFR1811 LEDs for troubleshooting purposes, perform a scan using the ZCT or push the Status Push Button on the ZFR1810 Coordinator.