Field Controller Model |
Plug the ZFR1811 Router Connector Cable into the Following Jack on the Field Controller: |
Connection Points for the Bluetooth® CVT Commissioning Interface and Other SA Bus Products |
Use this Communications Port between WEFC and Wired IOMs, WRZ Sensors, or VFDs: |
FAC26 | FC Bus RJ-12 Jack | SA Bus RJ-12 Jack | SA Bus Terminals |
FEC16 | FC Bus RJ-12 Jack | SA Bus RJ-12 Jack | SA Bus Terminals |
FEC26 | FC Bus RJ-12 Jack | SA Bus RJ-12 Jack | SA Bus Terminals |
IOM17 | SA/FC Bus RJ-12 Jack | Not available in wireless mode. Use CCT with ZFR Dongle. | N/A |
SA/FC Bus RJ-12 Jack | Not available in wireless mode. Use CCT with ZFR Dongle. | N/A | |
SA/FC Bus RJ-12 Jack | Not available in wireless mode. Use CCT with ZFR Dongle. | N/A | |
SA/FC Bus RJ-12 Jack | Not available in wireless mode. Use CCT with ZFR Dongle. | N/A | |
VMA1610/20 | SA Bus RJ-12 Jack | Use ZFRCBL Cable | FC Bus Terminals |
VMA1615/30 | FC Bus RJ-12 Jack | SA Bus RJ-12 Jack | SA Bus Terminals |
1 SA Bus Products include the DIS1710
Local Controller Display, the MS-BTCVT-1 Wireless Commissioning
Converter, and the NS Series (hard-wired) Network
Sensors, Balancing Sensors, and Discharge Air
Temperature Sensors.
2 IOMs cannot be used in wireless mode to extend
the IO of a field controller. You must always hardwire
FX-PCXss to their host field controller.
3 Do not connect any device to the SA
Bus/FC Bus terminal block when using the IOM
with a ZFR1811.