Application - Metasys - Part No. 24-10325-10 - Wireless Device - ZFR: Wireless Field Bus System - 5

ZFR1811 Wireless Field Bus Router Installation Instructions

Brand
Metasys
Product name
ZFR: Wireless Field Bus System
Document type
Installation Guide
Document number
Part No. 24-10325-10
Document revision
L
Version
5
Revision date
2017-02-01
Language
English

A ZFR1811 Wireless Field Bus Router is used with Field Equipment Advanced Application Controllers (FACs), Field Equipment Controllers (FECs), Input/Output Modules (IOMs), and Variable Air Volume Modular Assembly (VMA) Series field controllers.

The ZFR1811 Router provides a wireless interface between:

  • a field controller and the supervisory controller (by means of a ZFR1810 Coordinator)
  • a field controller and associated WRZ Series Wireless Room Sensors

Additionally, the ZFR1811 Wireless Field Bus Router can be used as a repeater in WRZ-7860-0 One-to-One Wireless Room Temperature Sensing System. For more information, refer to the WRZ Series One-to-One Wireless Room Sensing System Technical Bulletin (LIT-12011641).

Important: Use the ZFR1811 Wireless Field Bus Router only to provide an input to equipment under normal operating conditions. Where failure or malfunction of the ZFR1811 Router could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the ZFR1811 Router.
Important: The ZFR1800 Series Wireless Field Bus System is not designed or intended for use in mission-critical or life/safety applications.

Up to nine WRZ Series Sensors can be associated with a single field controller. In multi-sensor applications, the ZFR1811 Router passes all the sensor data to an FAC, FEC, IOM, or VMA controller, which can be configured to either average the sensors’ input or select the highest or lowest sensed condition for control of the target zone.

A ZFR1811 Router is powered directly from the connected field controller’s 15 VDC output.

The Router can also be powered by the power supply in the Repeater Accessory Kit to serve as a stand-alone repeater, extending the range of the communications within the wireless mesh network.

Refer to the ZFR1800 Series Wireless Field Bus System Technical Bulletin (LIT-12011295) for information about commissioning and configuring a ZFR1800 Series Wireless Field Bus System for operation.