Setup - Metasys - Wireless Device - ZFR-HPSST-0 Wireless Sensing System Tool

ZFR-HPSST-0 Wireless Sensing System Tool Installation Guide

Product
Network and Communications > Wireless Devices > ZFR-HPSST-0 Wireless Sensing System Tool
Document revision
C
Revision date
2023-03-08
Part number
24-11461-00012

Procedure

To set up both ZFR-HPSST-0 receivers that you use for the testing, perform the following steps:

  1. Install the batteries into the battery pack.
  2. Connect the battery pack wire harness to the two-pin connector located near the AREA switch of the ZFR1831.
  3. Move the W1 power jumper to the VBATT position (left two pins).
    Note: The ZFR1831-0 Router transforms into the ZFR-HPSST-0 tool when you connect the battery pack to the ZFR1831 Router. The ZFR1831 detects the battery and internally switches modes from normal Router operation to site survey tool operation.