Procedure
To set up both ZFR-HPSST-0 receivers that you use for the testing, perform
the following steps:
-
Install the batteries into the battery pack.
-
Connect the battery pack wire harness to the two-pin connector
located near the AREA switch of the ZFR1831.
-
Move the W1 power jumper to the VBATT position (left two
pins).
Note: The
ZFR1831-0 Router transforms into the ZFR-HPSST-0 tool when you connect the
battery pack to the ZFR1831 Router. The ZFR1831 detects the battery and
internally switches modes from normal Router operation to site survey tool
operation.