Repair information - Metasys - Wireless Device - ZFR-HPSST-0 Wireless Sensing System Tool

ZFR-HPSST-0 Wireless Sensing System Tool Installation Guide

Product
Network and Communications > Wireless Devices > ZFR-HPSST-0 Wireless Sensing System Tool
Document revision
C
Revision date
08/03/2023
Part number
24-11461-00012

If the ZFR-HPSST-0 Wireless Sensing System Tool fails to operate within its specifications, replace the unit. For a replacement ZFR-HPSST-0 Tool, contact the nearest Johnson Controls® representative.

Two AA alkaline batteries are supplied with the ZFR-HPSST-0Wireless Sensing System Tool. Replace the batteries with high-quality AA alkaline batteries as necessary, ensuring that the batteries are installed in the proper polarity. Replace both batteries at the same time.

Note: Batteries removed from this device must be recycled or disposed of in accordance with local, national, and regional regulations. Only certified technicians or qualified building maintenance personnel should service Johnson Controls products. Lithium batteries with a maximum cell voltage of 1.5 volts can be substituted to extend the period between battery replacement. Do not mix lithium and alkaline batteries in this device.