Operation - Metasys - Wireless Device - ZFR-HPSST-0 Wireless Sensing System Tool

ZFR-HPSST-0 Wireless Sensing System Tool Installation Guide

Product
Network and Communications > Wireless Devices > ZFR-HPSST-0 Wireless Sensing System Tool
Document revision
C
Revision date
08/03/2023
Part number
Part No. 24-11461-00012

Procedure

  1. When next to each other, turn both ZFR-HPSST-0 battery pack power switches to ON.
  2. Press and hold the join button on each unit to set their Tx power output. Release the button when in the required state, see Table 1. Both units should have the same setting.
    • Select 100 mW for ZFR1831 Router-Router/TEC3000 testing.
    • Select 10 mW for Router-Sensor testing.
    • Select 10 mW for ZFR181x or ZFR182x Router testing.
  3. Verify the LEDs go from an unpaired to a paired state, see Table 2.
  4. Place each ZFR-HPSST-0 device in a target location.
  5. Observe the LED pattern on either ZFR-HPSST-0, and refer to Table 2 to determine signal strength.
    Note: A red LED indicates a poor signal. Either use a better mounting location, if possible, or a repeater to achieve a stable wireless network.
  6. Once you determine the sites, turn the battery pack to the off position to conserve battery life.
    Table 1. LED Tx power
    Tx power LED color, pattern
    100 mW Mode Purple, rapid blink
    10 mW Mode Teal, rapid blink
    Table 2. LED Rx state
    Rx state LED color/pattern
    Unpaired Blue, rapid blink
    Paired, good signal Green, 3 blinks
    Paired, fair signal Yellow, 2 blinks
    Paired, poor or no signal Red, 1 blink